Page top

Primary Contents



Precautions for Correct Use of Photoelectric Sensors

Design

Power Reset Time

The Sensor will be ready to detect within approximately 100 ms after the power is turned ON.
If the Sensor and the load are connected to separate power supplies, turn ON the Sensor power before turning ON the load power. Any exceptions to this rule are indicated in Safety Precautions in individual product information.

Turning OFF Power

An output pulse may be generated when the power is turned OFF. It is recommended that the load or load line power be turned OFF before the Sensor power is turned OFF.

Power Supply Types

An unsmoothed full-wave or half-wave rectifying power supply cannot be used.

Mutual Interference

Mutual interference is a state where an output is unstable because the Sensors are affected by light from the adjacent Sensors.
The following measures can be taken to avoid mutual interference.

CountermeasureConceptThrough-beam SensorsReflective Sensors
1Use a Sensor with the interference prevention function.If Sensors are mounted in close proximity, use Sensors with the interference prevention function.
10 or fewer Sensors: E3X-DA[]-S, E3X-MDA, E3C-LDA Fiber Sensors
Performance, however, will depend on conditions. Refer to pages E3X-DA-S/E3X-MDA and E3C-LDA.
5 or fewer Sensors: E3X-NA Fiber Sensors
2 or fewer Sensors: E3T, E3Z, E3ZM, E3ZM-C, E3S-C, E3G-L1/L3, or E3S-C Built-in Amplifier Photoelectric Sensors (except Through-beam Sensors) E3C Photoelectric Sensor with separate amplifier
2Install an inference prevention filter.A mutual interference prevention polarizing filter can be installed on only the E3Z-TA to allow close-proximity mounting of up to 2 Sensors.
Mutual Interference Prevention Polarizing Filter: E39-E11
---
3Separate Sensors to distance where interference does not occur.Check the parallel movement distance range in the catalog, verify the set distance between adjacent Sensors, and install the Sensors accordingly at a distance at least 1.5 times the parallel movement distance range.If the workpieces move from far to near, chattering may occur in the vicinity of the operating point. For this type of application, separate the Sensors by at least 1.5 times the operating range.
4Alternate Emitters and Receivers.Close mounting of Sensors is possible by alternating the Emitters with the Receivers in a zigzag fashion (up to two Sensors). However, if the workpieces are close to the Photoelectric Sensors, light from the adjacent Emitter may be received and cause the Sensor to change to the incident light state.---
5Offset the optical axes.If there is a possibility that light from another Sensor may enter the Receiver, change the position of the Emitter and Receiver, place a light barrier between the Sensors, or take other measures to prevent the light from entering the Receiver. (Light may enter even if the Sensors are separated by more than the sensing distance.)If there is a possibility that light from another Sensor may enter the Receiver, change the position of the Emitter and Receiver, place a light barrier between the Sensors, or take other measures to prevent the light from entering the Receiver. (Light may enter even if the Sensors are separated by more than the sensing distance.)
6Adjust the sensitivity.Lowering the sensitivity will generally help.

Noise

Countermeasures for noise depend on the path of noise entry, frequency components, and wave heights. Typical measures are as given in the following table.

Type of noiseNoise intrusion path and countermeasure
Before countermeasureAfter countermeasure
Common mode noise
(inverter noise)
Common noise applied between the mounting board and the +V and 0-V lines, respectively.
Noise enters from the noise source through the frame (metal).(1) Ground the inverter motor (to 100 Ω or less)
(2) Ground the noise source and the power supply (0-V side) through a capacitor (film capacitor, 0.22 μF, 630 V).
(3) Insert an insulator (plastic, rubber, etc.) between the Sensor and the mounting plate (metal).
Radiant noise
Ingress of high-frequency electromagnetic waves directly into Sensor, from power line, etc.
Noise propagates through the air from the noise source and directly enters the Sensor.・ Insert a shield (copper) plate between the Sensor and the noise source e.g., a switching power supply).
・ Separate the noise source and the Sensor to a distance where noise does not affect operation.
Power line noise
Ingress of electromagnetic induction from high-voltage wires and switching noise from the switching power supply
Noise enters from the power line.・ Insert a capacitor (e.g., a film capacitor), noise filter (e.g.,ferrite core or insulated transformer), or varistor in the power line.

Wiring

Cable

Unless otherwise indicated, the maximum length of cable extension is 100 m using wire that is 0.3 mm2 or greater.
Exceptions are indicated in Safety Precautions in individual product information.

Cable Tensile Strength

When wiring the cable, do not subject the cable to a tension greater than that indicated in the following table.

Cable diameterTensile strength
Less than 4 mm30 N max.
4 mm or greater50 N max.

Note:Do not subject a shielded cable or coaxial cable to tension.

Repeated Bending

Normally, the Sensor cable should not be bent repeatedly.
(For bending-resistant cable, see Attachment to Moving Parts.)

Separation from High Voltage (Wiring Method)

Do not lay the cables for the Sensor together with high-voltage lines or power lines. Placing them in the same conduit or duct may cause damage or malfunction due to induction interference. As a general rule, wire the Sensor in a separate system, use an independent metal conduit, or use shielded cable.

Work Required for Unconnected Leads

Unused leads for self-diagnosis outputs or other special functions should be cut and wrapped with insulating tape to prevent contact with other terminals.

Power Supply

When using a commercially available switching regulator, ground the FG (frame ground) and G (ground) terminals.
If not grounded, switching noise in the power supply may cause malfunction.

Example of Connection with S3D2 Sensor Controller

DC Three-wire NPN Output Sensors

Reverse operation is possible using the signal input switch on the S3D2.

Mounting

Attachment to Moving Parts

To mount the Photoelectric Sensor to a moving part, such as a robot hand, consider using a Sensors that uses a bending-resistant cable (robot cable).

Although the bending repetition tolerance of a standard cable is approximately 13,000 times, robot cable has an excellent bending tolerance of approximately 500,000 times.

Cable Bending Destruction Test (Tough Wire Breaking Test)

With current flowing, bending is repeated to check the number of bends until the current stops.

SpecimenStandard cable VR (H) 3 x18/0.12Robot cable: Strong, conductive electrical wire 2 x 0.15 mm2, shielded
Test
Description/conditionsBending angle (θ)Left/right 90° eachLeft/right 45° each
Bending repetitions---60 bends/minute
Weight300g200g
Operation per bending(1) through (3) in figure once(1) through (3) in figure once
Bending radius of support points (R)5 mm2.5 mm
ResultApprox. 13,000 timesApprox. 500,000 times

The testing conditions of the standard cable and robot cable are different.
Refer to the values in the above table to check bend-resistant performance under actual working conditions.

Securing Fibers

The E3X Fiber Unit uses a one-touch locking mechanism. Use the following methods to attach and remove Fiber Units.

(1) Attaching Fibers

Open the protective cover, insert the fiber up to the insertion mark on the side of the Fiber Unit, and then lower the lock lever.

(2) Removing Fibers

Open the protective cover, lift up the lock lever, and pull out the fibers.

Note:1.To maintain the fiber characteristics, make sure that the lock is released before removing the fibers.
2. Lock and unlock the fibers at an ambient temperature of −10 to 40°C.

Adjustments

Optical Axis Adjustment

Move the Photoelectric Sensor both vertically and horizontally and set it in the center of the range in which the operation indicator is lit or not lit. For the E3S-C, the optical axis and the mechanical axis are the same, so the optical axis can be easily adjusted by aligning the mechanical axis.

Optical axis:

The axis from the center of the lens to the center of the beam for the Emitter and the axis from the center of the lens to the center of the reception area for the Receiver.

Mechanical axis:

The axis perpendicular to the center of the lens.

Operating Environment

Water Resistance

Do not use in water, in rain, or outside.

Ambient Conditions

Do not use this Sensor in the following locations. Otherwise, it may malfunction or fail.

(1) Locations exposed to excessive dust and dirt

(2) Locations exposed to direct sunlight

(3) Locations with corrosive gas vapors

(4) Locations where organic solvents may splash onto the Sensor

(5) Locations subject to vibration or shock

(6) Locations where there is a possibility of direct contact with water, oil, or chemicals

(7) Locations with high humidity and where condensation may result

Environmentally Resistive Sensors

The E32-T11F/T12F/T14F/T81F-S/D12F/D82F and E3HQ can be used in locations (3) and (6) above.

Optical Fiber Photoelectric Sensors in Explosive Gas Atmospheres

The Fiber Unit can be installed in the hazardous area, and the Amplifier Unit can be installed in a non-hazardous area.

<Reason>

For explosion or fire due to electrical equipment to occur, both the hazardous atmosphere and a source of ignition must be in the same location. Optical energy does not act as an ignition source, thus there is no danger of explosion or fire. The lens, case, and fiber covering are made of plastic, so this setup cannot be used if there is a possibility of contact with solvents that will corrode or degrade (e.g., cloud) the plastic.

<Ignition Source>

Electrical sparks or high-temperature parts that have sufficient energy to cause explosion in a hazardous atmosphere are called ignition sources.

Influence from External Electrical Fields

Do not bring a transceiver near the Photoelectric Sensor or its wiring, because this may cause incorrect operation.

Maintenance and Inspection

Points to Check When the Sensor Does Not Operate

If the Sensor does not operate, check the following points.

(1) Are the wiring and connections correct?

(2) Are any of the mounting screws loose?

(3) Are the optical axis and sensitivity adjusted correctly?

(4) Do the sensing object and the workpiece speed satisfy the ratings and specifications?

(5) Are any foreign objects, such as debris or dust, adhering to the Emitter lens or Receiver lens?

(6) Is strong light, such as sunlight (e.g., reflected from a wall), shining on the Receiver?

(7) Do not attempt to disassemble or repair the Sensor under any circumstances.

(8) If you determine that the Sensor clearly has a failure, immediately turn OFF the power supply.

Lens and Case

The lens and case of the Photoelectric Sensor are primarily made of plastic. Dirt should be gently wiped off with a dry cloth. Do not use thinner or other organic solvents.

The case of the E3ZM, E3ZM-C and E3S-C is metal. The lens, however, is plastic.

Accessories

Using a Reflector (E39-R3/R37/RS1/RS2/RS3) During Application

(1)When using adhesive tape on the rear face, apply it after washing
away oil and dust with detergent. The Reflector cannot be
mounted if there is any oil or dirt remaining.

(2) Do not press on the E39-RS1/RS2/RS3 with metal or a fingernail.This may weaken performance.

(3) This Sensor cannot be used in locations where oil or chemicals may splash on the Sensor.

M8 and M12 Connectors

Be sure to connect or disconnect the connector after turning OFF the Sensor.

Hold the connector cover to connect or disconnect the connector.

Secure the connector cover by hand. Do not use pliers, otherwise the connector may be damaged.

If the connector is not connected securely, the connector may be disconnected by vibration or the proper degree of protection of the Sensor may not be maintained.

Others

Values Given in Typical Examples

The data and values given as typical examples are not ratings and performance and do not indicate specified performance. They are rather values from samples taken from production lots, and are provided for reference as guidelines. Typical examples include the minimum sensing object, engineering data, step (height) detection data, and selection list for specifications.

Cleaning

Keep organic solvents away from the Sensor. Organic solvents will dissolve the surface.

Use a soft, dry cloth to clean the Sensor.