![]()
Global
These are navigation links to move inside this page.
|
|
| Precautions for Correct Use |
![]()
General notes
For notes for each product, see "Precautions" of each product.
Mounting
Displacement measurement of objects with differing materials and color.
If the material or color of objects is noticeably different, measurement error can be reduced by mounting the sensor so that the line joining the light projection axis and the light reception axis is parallel to the boundary line of the objects, as shown in the diagram below.
Measuring displacement in narrow grooves and depressions
If the object to be measured is in a depression or groove with wall-like sides, mount the sensor as shown in the diagram below so that the light projection axis and the light reception axis are not obstructed by the wall-like sides.
Displacement measurement of rotating objects
To measure rotating objects, the effects of vertical variations and positional variations can be minimized by mounting the sensor so that the line joining the light projection axis and the light reception axis is parallel to the axis of rotation.
Displacement measurement of objects with a step-like level difference.
If the object to be measured has a step-like level difference, the effects of the step edge can be minimized by mounting the sensor so that the line joining the light projection axis and the light reception axis is parallel to the step edge.
Sensor head and peripheral walls
Light reflected from a wall will cause error. If the sensor must be mounted near a wall, mount the sensor so that the line joining the light projection axis and the light reception axis is parallel to the wall, as shown in the diagram below. Painting the wall a dull black will also help reduce reflection.
If the object is black
If the object is black, there will be little light reflection, the value from the PSD will decrease, and the resolution will decrease.
The following mounting method is effective in increasing the absolute value of light reflected from the object.
Move head closer: Move the sensor head as close as possible within the range of the measurement distance to increase the projected and reflected light.
Receive light at the angle of regular reflection: Incline the sensor head when mounting so that the light reception axis is the same as the axis of regular reflecton with respect to the light projection axis.