Page top

Primary Contents


Precautions_for_Correct_use_fig

・ When using a Sensor that supports non-corrosive gas as the applicable fluid, use an air filter to remove moisture and oil from the gas.

・ Do not insert any wire or other object into the pressure port. Doing so may damage the pressure elements and cause a malfunction.

・ Do not use the Sensor alongside high-voltage lines or power lines.

・ Mount the Sensor so that it is not subject to ultrasonic vibration.

・ Do not apply a tensile force higher than 30 N to the cable or connector.

・ The cable can be extended to a maximum of 10 m. For details, see the output impedance section on the previous page.