![]()
Global
These are navigation links to move inside this page.
Programmable Digital Controller
A new High-speed, High-precision Digital Controller that is Programmable!
![]()
Quick links OMRON IA Temperature Controllers in your country.
Please contact Europe headquarters.
E5AR-T
Accessories (Optional)
Terminal Cover
E53-COV14 (for E5AR)
Unit Label Sheet
Y92S-L1
Rubber Packing
Y92S-P4 (for DIN96 × 96)
Order the Rubber Packing separately if it becomes lost or damaged.
(Deterioration, shrinking, or hardening of the rubber packing may occur depending on the operating environment. Therefore, periodic replacement is recommended to ensure the level of waterproofing specified in NEMA4. The time for periodic replacement depends on the operating environment. Be sure to confirm this point at your site. Consider one year a rough standard. OMRON shall not be liable for the level of water resistance if the customer does not perform periodic replacement.) The Rubber Packing does not need to be attached if a waterproof structure is not required.
Caution: All units are in millimeters unless otherwise indicated.