Page top

Primary Contents



H3M(-H)

H3M(-H)_Dim

Accessories (Order Separately)

Adapter with Flush Mounting

Y92F-40

Y92F-40_Dim

Note:When two or more timers mounted in line are to be continuously energized at the same time after the lapse of the set time, be sure to limit the carry current to less than 1 A. When using the timers at an ambient temperature of more than 40°C, be sure to reset the timers immediately after the set time has elapsed.

Track Mounted/Front Connecting Socket

PF085A

PF085A_Dim

Hold-down Clips (Attached)

PHC-1 For PF085A

PHC-1 For PF085A_Dim

Back Connecting Socket

PL08

PL08_Dim

P3G-08

P3G-08_Dim

Caution: All units are in millimeters unless otherwise indicated.