![]()
Global
These are navigation links to move inside this page.
The High-performance Vision Sensor
An unending Quest for Faster Processing Combined with Years of Know-how, New Functions for Improved Production Processes
![]()
Quick links to 'F270' page in your country / territory.
Please contact our European headquarters.
Get more support via Products links, such as manuals and CAD files.
Select the mode for operation.
A mode for high-speed measurements or A mode to add more inspection items and increase measurement accuracy.
Use the One-line High-speed Mode.
With the world's fastest processing speed, even more detailed inspections are possible.
For inspections at multiple stages of production and reduced space requirements.
Use the Random Trigger Mode.
The work of two Controllers can be performed by only one Controller.
QUEST Character and Lot Number Vertification
Variation in characters reduces inspection accuracy.
The F270 saves a lot of working hours spent registering characters in dictionaries and registering models.
EC Positioning
Considerably higher measurement accuracy than conventional measurement methods.
EC positioning
Repeatability:1/20 pixel
(OMRON test data,The measurement accuracy will depend on the actual workpiece. Check the accuracy before using the F270)
Stable measurement of variations in shape and contrast.
Inspection of Defects, Scratches, and Dirt
Conventional fixed-area inspections did not provide stable measurements.
Effective for workpieces with tolerances and workpieces with shape variations.
Effective for detecting minute foreign objects or dirt on complicated backgrounds.