Page top

ES2-HB / THB

Humidity Sensor, Temperature/Humidity Sensor

ES2-HB / THB

Detect Humidity within an Accuracy of ±3% in a Compact Body. Controller Set Provides Superior Humidity Control and Temperature/Humidity Control.

Name Model
Humidity Sensor ES2-HB
Temperature/Humidity Sensor ES2-THB
Humidity Sensor Module * ES2-M
* This is a replacement item. One Module is provided with the ES2-HB/-THB. Always attach the Humidity Sensor Module
    when using the ES2-HB/-THB. Approximately 7 VDC will be output for the humidity output if the Module is not attached
    or is incompletely attached.