Page top

H3M

Solid-state Timer

H3M

Solid-state Timer with Variable Time Ranges

Caution: All units are in millimeters unless otherwise indicated.

H3M(-H)

H3M Dimensions 1

Accessories (Order Separately)

Adapter with Flush Mounting

Y92F-40

H3M Dimensions 4

Note: When two or more timers mounted in line are to be continuously energized at the same time after the lapse of the
          set time, be sure to limit the carry current to less than 1 A. When using the timers at an ambient temperature of
          more than 40°C, be sure to reset the timers immediately after the set time has elapsed.

Track Mounted/Front Connecting Socket

PF085A

H3M Dimensions 6

Note: There are no restrictions to the mounting direction.

Hold-down Clips (Attached)

PHC-1 For PF085A

H3M Dimensions 8

Back Connecting Socket

PL08

H3M Dimensions 10

P3G-08

H3M Dimensions 11