Page top

CJ1M-CPU1[]-ETN

SYSMAC CJ-series CJ1M CPU Units (with Ethernet function)

CJ1M-CPU1[]-ETN

A Micro CJ1M CPU Unit with Built-in Ethernet Newly Released!

Common Specifications

Item Specifications
Control method Stored program
I/O control method Cyclic scan and immediate processing are both possible.
Programming Languages Ladder Logic (LD), Sequential Function Charts (SFC), Structured Text (ST), and
Mnemonic.
CPU processing mode Normal Mode or Peripheral Servicing Priority Mode
Instruction length 1 to 7 steps per instruction
Ladder instructions Approx. 400 (3-digit function codes)
Execution
time
Basic instructions 0.10 μs min.
Special
instructions
0.15 μs min.
Overhead time CJ1M-CPU12-ETN/CPU13-ETN: 0.5 ms min.
CJ1M-CPU11-ETN: 0.7 ms min.
Unit connection method No Backplane: Units connected directly to each other.
Mounting method DIN Track (screw mounting not possible)
Maximum number of
connectable Units
Total of 19 Units, including 9 Units on CPU Rack and 10 Units on one Expansion
Rack.
(The built-in Ethernet port on the CPU Unit must be allocated to a slots 0, and is
counted as one Unit.)
Maximum number of Expansion
Racks
CJ1M-CPU13-ETN: 1 max. (An I/O Control Unit is required on the CPU Rack and
an I/O Interface Unit is required on the Expansion Rack.)
CJ1M-CPU11-ETN/12-ETN: Expansion is not possible.
Number of tasks 288 (cyclic tasks: 32, interrupt tasks: 256)
With CJ1-H or CJ1M CPU Units, interrupt tasks can be defined as cyclic tasks
called extra cyclic tasks. Including these, up to 288 cyclic tasks can be used.
Cyclic tasks are executed each cycle and are controlled with TKON (820) and
TKOF (821) instructions.
Note 1.
The following 4 types of interrupt tasks are supported.
Note 2.
Power OFF interrupt tasks: 1 max.
Scheduled interrupt tasks: 2 max.
I/O interrupt tasks: 32 max.
External interrupt tasks: 256 max.
Interrupt types Scheduled Interrupts: Interrupts generated at a time scheduled by the CPU Units
built-in timer.
I/O Interrupts: Interrupts from Interrupt Input Units.
Power OFF Interrupts (See note): Interrupts executed when the CPU Units power
is turned OFF.
External I/O Interrupts: Interrupts from the Special I/O Units or CPU Bus Units.
Note: Not supported when the CJ1W-PD022 Power Supply Unit is mounted.
Calling subroutines from more
than one task
Supported (called global subroutines).
CIO
(Core I/O)
Area
I/O Area 2,560: CIO 000000 to CIO 015915 (160 words from CIO 0000 to
CIO 0159)
The setting of the first word can be changed from the default (CIO
0000) so that CIO 0000 to CIO 0999 can be used.
I/O bits are allocated to Basic I/O Units.
The CIO Area
can be used
as work bits
if the bits are
not used as
shown here.
Link Area 3,200 (200 words): CIO 10000 to CIO 119915 (words CIO 1000 to
CIO 1199)
Link bits are used for data links and are allocated to Units in
Controller Link Systems.
CPU Bus Unit Area 6,400 (400 words): CIO 150000 to CIO 189915 (words CIO 1500 to
CIO 1899)
CPU Bus Unit bits store the operating status of CPU Bus Units.
(25 words per Unit, 16 Units max.)
Special I/O Unit
Area
15,360 (960 words): CIO 200000 to CIO 295915 (words CIO 2000
to CIO 2959)
Special I/O Unit bits are allocated to Special I/O Units. (10 words
per Unit, 96 Units max.)
Serial PLC Link
Area (CJ1M CPU
Units only)
1,440 (90 words): CIO 310000 to CIO 318915 (words CIO 3100 to
CIO 3189)
DeviceNet Area 9,600 (600 words): CIO 320000 to CIO 379915 (words CIO 3200 to
CIO 3799)
DeviceNet bits are allocated to Slaves for DeviceNet Unit remote
I/O communications when the Master function is used with fixed
allocations.
Fixed allocation setting 1 Outputs: CIO 3200 to CIO 3263
Inputs: CIO 3300 to CIO 3363
Fixed allocation setting 2 Outputs: CIO 3400 to CIO 3463
Inputs: CIO 3500 to CIO 3563
Fixed allocation setting 3 Outputs: CIO 3600 to CIO 3663
Inputs: CIO 3700 to CIO 3763
The following words are allocated to the Master function even
when the DeviceNet Unit is used as a Slave.
Fixed allocation setting 1 Outputs: CIO 3370 (Slave to Master)
Inputs: CIO 3270 (Master to Slave)
Fixed allocation setting 2 Outputs: CIO 3570 (Slave to Master)
Inputs: CIO 3470 (Master to Slave)
Fixed allocation setting 3 Outputs: CIO 3770 (Slave to Master)
Inputs: CIO 3670 (Master to Slave)
Internal I/O Area 4,800 bits (300 words): CIO 120000 to CIO 149915 (words CIO 1200 to CIO 1499)
37,504 (2,344 words): CIO 380000 to CIO 614315 (words CIO 3800 CIO 6143)
These bits in the CIO Area are used as work bits in programming to control
program execution. They cannot be used for external I/O.
Work Area 8,192 bits (512 words): W00000 to W51115 (W000 to W511)
Controls the programs only. (I/O from external I/O terminals is not possible.)
Note: When using work bits in programming, use the bits in the Work Area first
before using bits from other areas.
Holding Area 8,192 bits (512 words): H00000 to H51115 (H000 to H511) Holding bits are used to
control the execution of the program, and maintain their ON/OFF status when the
PLC is turned OFF or the operating mode is changed.
Note: The Function Block Holding Area words are allocated from H512 to H1535.
These words can be used only for the function block instance area (internally
allocated variable area).
Auxiliary Area Read only: 7,168 bits (448 words): A00000 to A44715 (words A000 to A447)
Read/write: 8,192 bits (512 words): A44800 to A95915 (words A448 to A959)
Auxiliary bits are allocated specific functions.
Temporary Area 16 bits (TR0 to TR15)
Temporary bits are used to temporarily store the ON/OFF execution conditions at
program branches.
Timer Area 4,096: T0000 to T4095 (used for timers only)
Counter Area 4,096: C0000 to C4095 (used for counters only)
DM Area 32 Kwords: D00000 to D32767
Used as a general-purpose data area for reading and writing data in word units (16
bits). Words in the DM Area maintain their status when the PLC is turned OFF or
the operating mode is changed.
Internal Special I/O Unit DM Area: D20000 to D29599 (100 words × 96 Units)
Used to set parameters for Special I/O Units.
CPU Bus Unit DM Area: D30000 to D31599 (100 words × 16 Units)
Used to set parameters for CPU Bus Units.
EM Area None
Index Registers IR0 to IR15
Store PLC memory addresses for indirect addressing. Index registers can be used
independently in each task.
One register is 32 bits (2 words).
Setting to use index registers either independently in each task or to share them
between tasks.
Task Flag Area 32 (TK0000 to TK0031)
Task Flags are read-only flags that are ON when the corresponding cyclic task is
executable and OFF when the corresponding task is not executable or in standby
status.
Trace Memory 4,000 words (trace data: 31 bits, 6 words)
File Memory Memory Cards: Compact flash memory cards can be used (MS-DOS format).
OMRON Memory Cards can be used.
Function
Specifi-
cations
Constant cycle
time
1 to 32,000 ms (Unit: 1 ms)
Cycle time
monitoring
Possible (Unit stops operating if the cycle is too long): 10 to 40,000 ms (Unit: 10
ms)
I/O refreshing Cyclic refreshing, immediate refreshing, refreshing by IORF (097).
Note: ORF (097) refreshes I/O bits allocated to Basic I/O Units and Special I/O
Units.
Timing of special
refreshing for CPU
Bus Units
Data links for Controller Link Units remote I/O for DeviceNet Units, and other
special refreshing for CPU Bus Units is performed at the following times:
I/O refresh period and when the CPU BUS UNIT I/O REFRESH (DLNK (226))
instruction is executed.
I/O memory holding
when changing
operating modes
Depends on the ON/OFF status of the IOM Hold Bit in the Auxiliary Area.
Load OFF All outputs on Output Units can be turned OFF when the CPU Unit is operating in
RUN, MONITOR, or PROGRAM mode.
Timer/Counter PV
refresh method
BCD or binary (CX-Programmer Ver. 3.0 or higher).
Input response
time setting
Time constants can be set for inputs from Basic I/O Units.
The time constant can be increased to reduce the influence of noise and
chattering or it can be decreased to detect shorter pulses on the inputs.
Mode setting at
power-up
Possible.
Note: By default, the CPU Unit will start in RUN mode if a Programming Console is
not connected.
Flash memory
(CJ1-H and CJ1M
CPU Units only)
The user program and parameter area data (e.g., PLC Setup) are always backed up
automatically in flash memory. (automatic backup and restore.)
CPU Units with unit version 3.0 or later only:
When downloading projects from CX-Programmer Ver. 5.0 or higher, symbol table
files (including CX-Programmer symbol names, I/O comments), comment files
(CX-Programmer rung comments, other comments), and program index files (CX-
Programmer section names, section comments, or program comments) are stored
in comment memory within the flash memory.
Memory Card
functions
Automatically reading
programs (autoboot) from
the Memory Card when the
power is turned ON.
Possible.
Program replacement
during PLC operation
Possible.
Format in which data is
stored in Memory Card
User program: Program file format PLC Setup and
other parameters: Data file format I/O memory: Data
file format (binary format), text format, or CSV format
Functions for which
Memory Card read/write is
supported
User program instructions, Programming Devices
(including CX-Programmer and Programming
Consoles), Host Link computers, AR Area control
bits, easy backup operation
Filing Memory Card data and the EM (Extended Data Memory) Area can be handled as
files.
Debugging Control set/reset, differential monitoring, data tracing (scheduled, each cycle, or
when instruction is executed), instruction error tracing, storing location
generating error when a program error occurs.
Online editing User programs can be overwritten in program-block units when the CPU Unit is in
MONITOR or PROGRAM mode.
This function is not available for block programming areas.
With the CX-Programmer, more than one program block can be edited at the same
time.
Program
protection
Overwrite protection: Set using DIP switch.
Copy protection: Password set using CX-Programmer or Programming Consoles.
Error check User-defined errors (i.e., user can define fatal errors and non-fatal errors)
The FPD(269) instruction can be used to check the execution time and logic of
each programming block.
Note: FAL and FALS instructions can be used with the CJ1-H and CJ1M CPU
Units to simulate errors.
Error log Up to 20 errors are stored in the error log. Information includes the error code,
error details, and the time the error occurred.
Note: CJ1M CPU Unit can be set so that user-defined FAL errors are not stored
in the error log.
Serial
communications
Built-in peripheral port: Programming Device (including Programming Console)
connections, Host Links, NT Links, Serial Gateway (CompoWay/F master)
Built-in RS-232C port: Programming Device (excluding Programming Console)
connections, Host Links, no-protocol communications, NT Links, Modbus-RTU
Slave, Serial Gateway (CompoWay/F master or Modbus master)
Serial Communications Unit (sold separately): Protocol macros, Host Links, NT
Links
Clock Provided on all models.
Accuracy:
Ambient temperature Monthly error
55°C -3.5 min to +0.5 min
25°C -1.5 min to +1.5 min
0°C -3 min to +1 min
Note: Used to store the time when power is turned ON and when errors occur.
Power OFF
detection time
AC Power Supply Unit: 10 to 25 ms (not fixed)
DC Power Supply Unit PD025: 2 to 5 ms; PD022: 2 to 10 ms
Power OFF
detection delay
time
0 to 10 ms (user-defined, default: 0 ms)
Note: Not supported when the CJ1W-PD022 Power Supply Unit is mounted.
Memory protection Held Areas: Holding bits, contents of Data Memory and Extended Data Memory, and
status of the counter Completion Flags and present values.
Note:
If the IOM Hold Bit in the Auxiliary Area is turned ON, and the PLC Setup is set to
maintain the IOM Hold Bit status when power to the PLC is turned ON, the
contents of the CIO Area, the Work Area, part of the Auxiliary Area, timer
Completion Flag and PVs, Index Registers, and the Data Registers will be saved for
up to 20 days.
Sending
commands to a
Host Link
computer
FINS commands can be sent to a computer connected via the Host Link System
by executing Network Communications Instructions from the PLC.
Remote
programming and
monitoring
Host Link communications can be used for remote programming and remote
monitoring through a Controller Link System or Ethernet network.
Communicating
across
network levels
Remote programming and monitoring from Support Software and FINS message
communications can be performed across different network levels, even for
different types of network.
Pre-Ver. 2.0: Three levels
Version 2.0 or later: Eight levels for Controller Link and Ethernet networks (See
note.), three levels for other networks.
Note: To communicate across eight levels, the CX-Integrator or the CX-Net in
Programmer version 4.0 or higher must be used to set the routing tables.
Storing comments
in CPU Unit
I/O comments can be stored as symbol table files in the Memory Card, EM file
memory, or comment memory (see note).
Note: Comment memory is supported for CX-Programmer version 5.0 or higher
and CS/CJ-series CPU Units with unit version 3.0 or later only.
Program check Program checks are performed at the beginning of operation for items such as no
END instruction and instruction errors.
CX-Programmer can also be used to check programs.
Control output
signals
RUN output: The internal contacts will turn ON (close) while the CPU Unit is
operating (CJ1W-PA205R).
Battery life Battery Set for CJ1M CPU Units: CJ1W-BAT01
Self-diagnostics CPU errors (watchdog timer), I/O bus errors, memory errors, and battery errors.
Other functions Storage of number of times power has been interrupted. (Stored in A514.)

Ethernet Functional Element Transfer Specifications

Item Specifications
Model CJ1M-CPU11-ETN CJ1M-CPU12-ETN CJ1M-CPU13-ETN
Media access method CSMA/CD
Modulation method Baseband
Transmission paths Star form
Baud rate 100 Mbit/s (100Base-TX), 10 Mbit/s (10Base-T)
Transmission media 100 Mbit/s Unshielded twisted-pair (UDP) cable Categories: 5, 5e
Shielded twisted-pair (STP) cable Categories: 100 Ω at 5, 5e
10 Mbit/s Unshielded twisted-pair (UDP) cable Categories: 3, 4, 5, 5e
Shielded twisted-pair (STP) cable Categories: 100 Ω at 3, 4, 5, 5e
Transmission distance 100 m (distance between hub and node)
Number of cascade connections There are no restrictions with the use of switching hubs.
CPU Bus Unit System Setup Area capacity 994 bytes

Note: The system settings for Ethernet are in the CPU Bus Unit System Setup Area in the CPU Unit.