- One machine control to ensure high precision synchronization between conveyor and robot
- High-speed control, from sensor inputs to robot control
- Control of even manipulators synchronized with robot motion via EtherCAT
NJ-series NJ Robotics CPU Units
last update: July 20, 2017
When building conveyor tracking applications, you can program Pick & Place control systems by using the same program structure in the same programming manner regardless of the robot type: parallel, Cartesian , or SCARA robot.
You can perform integrated simulations linked to motion control for robots and inspection and measurement by vision systems.
The virtual environment allows to visualize the machine motion.
The simulation of the synchronization between robots makes complex operation verification easy.
Machine movement can be simulated based on measurement results of vision systems.
* Only Delta3 and Delta3R robots can be used for integrated simulation.
Adjusting, monitoring parameters of the robot’s drives is done easily in a single view.
Several 1S servo drives can be tuned simultaneously in a short amount of time.
Far from the old and rigid top-down programming manner our solution is based on Wizards that guide the user through the main steps using a graphical interface to operate with an unique software tool capable to manage Robotics and Vision seamlessly at the same time.
Virtualize your Pick & Place machine into the integrated 3D Simulator and make it Real in 5 simple steps, guided by intuitive wizards.
Image capturing
• The first step is to take the pictures of the products to handle. Yes just as easy as it sounds!
• The wide portfolio of our FH cameras allows to optimize your choice.
[Patented] Import the pictures into Sysmac Studio wizard
• Using the Sysmac Studio wizard you can define the layout of the Pick & Place machine, selecting how many robots and conveyors you have and choose between the most typical layout templates.
[Patented] 3D Simulation
• Sysmac Studio generates the 3D simulation environment according to the parameters defined in the previous steps.
• The integrated graphical environment enables visualizing the Pick & Place machine and the Vision simulation at the same time.
• Moreover, the images captured in the Step 1 are automatically converted into the corresponding virtual products that run over the picking conveyor.
Reuse of codes
• The 3D simulation is very reliable since it is based on the real system cores so you can reuse the whole programming to control the real machine by significantly shortening the commissioning time.
[Patent Pending] Easy tuning on site P&P and FH Vision
• The finalization of your project is guided by a Vision system wizard that calibrates the Virtual machine against the Real machine.
• It take just few minutes to place a matrix calibration sheet into the machine and follow the wizard that will align the robots and the vision systems to minimize any kind of measurement error.
Sysmac is a trademark or registered trademark of OMRON Corporation in Japan and other countries for OMRON factory automation products.
Windows is registered trademarks of Microsoft Corporation in the USA and other countries.
EtherCAT® is a registered trademark of Beckhoff Automation GmbH for their patented technology.
EtherNet/IPTM, DeviceNetTM are trademarks of the ODVA.
Other company names and product names in this document are the trademarks or registered trademarks of their respective companies.
last update: July 20, 2017