(Unit: mm)
Digital Counter
You can download software for the H7CC.
last update: May 22, 2023
(Unit: mm)
H7CC-A8/-A8D (Flush Mounting/Surface Mounting Models)
H7CC-A11/-A11S/-A11D/-A11SD (Flush Mounting/Surface Mounting Models)
H7CC-A/-AS/-AD/-ASD/-AW/-AWS/-AWD/-AWSD/-AU/-AUD
(Provided with Adapter and Waterproof packing)
H7CC-A8/-A8D/-A11/-A11S/-A11D/-A11SD
(Flush Mounting/Surface Mounting Models)
(Adapter and Waterproof packing Ordered Separately)
Panel cutouts are as shown below. (according to DIN43700).
Note:
1. The mounting panel thickness should be 1 to 5 mm.
2. To allow easier operation, it is recommended that Adapters be mounted so that the gap between sides with hooks is at least 15 mm (i.e., with the panel cutouts separated by at least 60 mm).
3. It is possible to horizontally mount Timers side by side. Attach the Flush Mounting Adapters so that the surfaces without hooks are on the sides of the Timers. If they are mounted side-by-side, waterresistance will be lost.
* These dimensions depend on the kind of DIN track and Sockets. (Reference value.)
Note: Depending on the operating environment, the condition of resin products may deteriorate, and may shrink or become harder. Therefore, it is recommended that resin products are replaced regularly.
Soft Cover
Y92A-48F1
Hard Cover
Y92A-48
The H7CC's panel surface is water-resistive (conforming to IP[]6) and so even if drops of water penetrate the gaps between the keys, there will be no adverse effect on internal circuits. If, however, there is a possibility of oil being present on the operator's hands, use the Soft Cover. The Soft Cover ensures protection equivalent to IP54F against oil. Do not, however, use the H7CC in locations where it would come in direct contact with oil.
Waterproof Packing
Y92S-P6
Note: The Waterproof Packing is included with models with screw terminals.
Order the Waterproof Packing separately if it is lost or damaged. The Waterproof Packing can be used to achieve IP66 protection.
The panel surface of the H7CC-A/-R is water-resistant (conforming to IP66). To protect the internal circuits from water penetration through the space between the H7CC and operating panel, waterproof packing is included. Attach the Y92F-30 Adapter with sufficient pressure with the reinforcing screws so that water does not penetrate the panel.
The Waterproof Packing will deteriorate, harden, and shrink depending on the application environment. To ensure maintaining the IP[]6 waterproof level, periodically replace the Waterproof Packing.
The periodic replacement time will depend on the application environment. You must confirm the proper replacement time. Use 1 year or less as a guideline. If the Waterproof Packing is not replaced periodically, the waterproof level will not be maintained. It is not necessary to mount the Waterproof Packing if waterproof construction is not required.
Flush Mounting Adapter
Y92F-30
Order the Flush Mounting Adapter with the following model number separately if it is lost or damaged.
Note: The Waterproof Packing is included with models with screw terminals.
Note:
1. The adapter is black in color.
2. The Y92F-45 can be used in combination with the Y92F-30 Adapter provided with the Counter.
H7CC Mounting Example
P2CF-11
P2CF-11-E
(Finger-safe Type)
P2CF-08
P2CF-08-E
(Finger-safe Type)
Note: Round crimp terminals cannot be used on Finger-safe Sockets. Use forked crimp terminals.
P3GA-11
Note: A Y92A-48G Terminal Cover can be used with the Socket to create a finger-safe construction.
Y92A-48G
Note: The Terminal Cover can be used with a Back-mounting Socket (P3GA-11, P3G-08) to create a finger-safe construction.
Mounting Track
PFP-100N
PFP-50N
Mounting Track
PFP-100N2
End Plate
PFP-M
Spacer
PFP-S
Note: Order Spacers in increments of 10.
last update: May 22, 2023