Page top

K7L-AT50[] / AT50D[][]

Liquid Leakage Sensor Amplifier/Liquid Leakage Sensor Amplifier with Disconnection Detection Function

K7L-AT50[] / AT50D[][]

Reliable Detection of a Wide Variety of Liquids Ranging from Water to Liquid Chemicals with Low Conductivity. Four Sensing Ranges Available. K7L-AT50B and K7L-AT50DB are our Value Design products which increase the value of your control panels.

(Unit: mm)

Liquid Leakage Sensor Amplifier

K7L-AT50/AT50D/AT50DP

K7L-AT50[] / AT50D[][] Dimensions 1

Liquid Leakage Sensor

K7L-AT50B/AT50DB/AT50DPB

K7L-AT50[] / AT50D[][] Dimensions 2

Terminal Block *

F03-20

K7L-AT50[] / AT50D[][] Dimensions 3

* The Terminal Block is made of nylon 66. Mount the Terminal Block in locations not subject to liquid chemicals using M3
  screws.

Terminator *

F03-20T

K7L-AT50[] / AT50D[][] Dimensions 5

* The Terminal Block is made of nylon 66. Mount the Terminal Block in locations not subject to liquid chemicals using M3
  screws.

Track-mounted Sockets *

P2RF-08 (Round terminals can be used.)

K7L-AT50[] / AT50D[][] Dimensions 7

Note: Secure the Sockets with M3 screws at a torque of 0.78 to 1.18 N⋅m.
* The applicable models of the K7L depend on the model of the Socket. If the correct Socket is not used, the K7L nameplate will be upside down.

Track-mounted Sockets *

P2RF-08-E

K7L-AT50[] / AT50D[][] Dimensions 9

Note: Secure the Sockets with M3 screws at a torque of 0.78 to 1.18 N⋅m.
* The applicable models of the K7L depend on the model of the Socket. If the correct Socket is not used, the K7L nameplate will be upside down.

Track-mounted Sockets

P2RF-08-PU

K7L-AT50[] / AT50D[][] Dimensions 11

Note: The applicable models of the K7L depend on the model of the Socket. If the correct Socket is not used, the K7L nameplate will be upside down.

Liquid Leakage Point Sensor

F03-16PS
F03-16PS-F

K7L-AT50[] / AT50D[][] Dimensions 13

Point Sensor Mounting Bracket

F03-26PS

K7L-AT50[] / AT50D[][] Dimensions 14

* Use a commercially available bonding agent for PVC.Do not use adhesive tape for securing.