Page top

Lead Contents

FAQ02413 of Safety Sensors FAQ

FAQ No. FAQ02413

Primary Contents

Question

What is an auxiliary output?

Answer



F3SN/F3SH Series Safety Light Curtains

The default setting of the output is the reverse signal of the control output. It is only an auxiliary output, so do not use it as a control output for a safety circuit.

For F3SN-A and F3SH Series, the output operation mode can be selected using F39-MC11 Setting Console.

Dark-ON output = Control output and its reverse signal (default setting)

Light-ON output = Synchronized with the control output

Light diagnosis output

Lockout output

Outermost-beam monitoring output

Specified-beam output

Blanking monitoring output (F3SN-A only)

F3SL Series Safety Light Curtain

A signal is output in sync with the control output. It is only an auxiliary output, so do not use it as a control output for a safety circuit.

Recommended Products

F3SR-B

For Safety Light Curtain Robust & Basic New Lineup. Understanding the Indicators at a Glance.

OS32C

Compact (104.5 mm), lightweight (1.3 kg) and easy-to-install Safety Laser Scanner

D40Z

Supports ISO 13849-1 (PLe/Safety Category 4). Can be used on higher risk level applications by connecting to Safety Controllers.

Other Safety Sensors FAQ