Page top

Lead Contents

FAQ02417 of Safety Sensors FAQ

FAQ No. FAQ02417

Primary Contents


What is a manual reset?


A manual reset is a selectable feature of the interlock function.

When the Safety Sensor enters the interlock state, it keeps the control outputs in the OFF state. Even if all beams become free, the control outputs will not go to the ON state.

When none of the beams are interrupted in the detection zone and it is safe to operate the device, applying the reset input will reset the interlock condition and the control outputs will go to the ON state.

Applicable models:

F3SN Series Safety Light Curtain

F3SH Series Multi Beam Safety Sensor

Recommended Products


For Safety Light Curtain Robust & Basic New Lineup. Understanding the Indicators at a Glance.


Compact (104.5 mm), lightweight (1.3 kg) and easy-to-install Safety Laser Scanner


Supports ISO 13849-1 (PLe/Safety Category 4). Can be used on higher risk level applications by connecting to Safety Controllers.

Other Safety Sensors FAQ