Page top

Lead Contents

FAQ00868 of Counters FAQ

FAQ No. FAQ00868

Primary Contents

Question

When a single pulse only is input in the Counter, why does the Counter convert the pulse into at least two count values?

Answer



The following two causes may be causing in this problem.

1. The maximum counting speed setting is set to high-speed response and the Counter may be receiving relay chattering, bouncing, or noise input.

Countermeasure:

Set the maximum counting speed to as lower speed.

2. If the Counter has a prescaling function, the prescale value may be set.

Countermeasure:

Check whether the prescale value is set.

Recommended Products

K3HB-X

A Process Indicator Ideal for Discriminating and Displaying Measurements for Voltage/Current Signals

E5CN-H

A New High-performance Controller: High Resolution, High Speed, and High Input Accuracy. Logic Operations and Preventive Maintenance Function.

H5CZ

Easy to Use and Easy to Read.

Other Counters FAQ