Page top

Lead Contents

FAQ00875 of Counters FAQ

FAQ No. FAQ00875

Primary Contents


Why is the top section of the display not showing on the H5CN-[][][]M/H7CN-[][][]M Counter?


If a power interruption to the Counter occurs for 10 minutes or longer with the battery disconnected, errors will occur in the count value and display, even if the power recovers. Make sure a battery is connected to the Counter if the model has the suffix -M (backup function for power interruptions).

Any battery supplying 3 V can be used, but the data backup time depends on the capacity of the battery.

Recommended Products


A Process Indicator Ideal for Discriminating and Displaying Measurements for Voltage/Current Signals


A New High-performance Controller: High Resolution, High Speed, and High Input Accuracy. Logic Operations and Preventive Maintenance Function.


Easy to Use and Easy to Read.

Other Counters FAQ