Page top

Lead Contents

FAQ03598 of Counters FAQ

FAQ No. FAQ03598

Primary Contents

Question

When the H7ET-N's Time Counters time range switch is set to 0.0 to 3999d23.9h, what is displayed after 23.9 h?

Answer



100.0 will be displayed after 23.9.
100.0 signifies 1 (day) and 00.0 (hour).
For example, one day and 1.0 hour would be displayed as 101.0.

Supplementary Information
0.1 h indicates 6 minutes.
Therefore, 0.0 will be displayed between 0 to 5 minutes, and 0.1 will be displayed after 6 minutes.

Note:

1.Set the switches before mounting the Unit to a control panel.

2.If the counting speed setting is changed, the present value will not be held. Press the Reset Key on the front panel.

The time unit is given in the datasheet and in the figure above, but on the actual device it will not be displayed. Instead, unit labels (-hours/-d-h/-h-m/-h-m-s) are provided.

Recommended Products

K3HB-X

A Process Indicator Ideal for Discriminating and Displaying Measurements for Voltage/Current Signals

E5CN-H

A New High-performance Controller: High Resolution, High Speed, and High Input Accuracy. Logic Operations and Preventive Maintenance Function.

H5CZ

Easy to Use and Easy to Read.

Other Counters FAQ