![]()
Global
These are navigation links to move inside this page.
![]()
Quick links to OMRON IA in your country / territory.
Please contact our European headquarters.
Question
Why was the Sensor output damaged when the Timer power was turned ON/OFF?
Answer
When the power was applied, the inrush current from the Timer may have damaged the Sensor output.
Countermeasure:
Use the MY Relay or other relay to turn the Timer power supply ON/OFF. (Make sure that the contact capacity is sufficient.)
New 48 x 48-mm Basic Temperature Controller with Enhanced Functions and Performance. Improved Indication Accuracy and Preventive Maintenance Function.
Multiple Operating Modes and Multiple Time Ranges. DIN 48 x 48-mm Multifunctional Timer with Wide AC/DC Power Supply Range for Both High and Low Voltages.
DIN 48 × 48-mm Multifunction Digital Timer/2-stage Digital Timer