Page top

Primary Contents

Question

Why can't AC 2-Wire Proximity Sensors switch the Timers power supply?

Answer



Probable Cause 1

Some Timers have half-wave rectifiers built into their power supply circuits. In this case, only half of the AC voltage will be supplied to Sensors and Sensors will not operate. Therefore it cannot be used to operate Timers.

Countermeasure
Instead of using Proximity Sensors, use Relays such as MY2N-CR General Purpose Relays to switch Timers power supply. (Pay careful attention to the contact capacity.)

Probable Cause 2

The Sensors output may have been damaged due to Timers inrush current when the power was turned ON.

Countermeasure
Instead of using Proximity Sensors, use Relays such as MY2N-CR to switch Timers power supply. (Pay careful attention to the contact capacity.)

Recommended Products

E5CN/E5CN-U (48 x 48 mm)

New 48 x 48-mm Basic Temperature Controller with Enhanced Functions and Performance. Improved Indication Accuracy and Preventive Maintenance Function.

H3CR-A

Multiple Operating Modes and Multiple Time Ranges. DIN 48 x 48-mm Multifunctional Timer with Wide AC/DC Power Supply Range for Both High and Low Voltages.

H5CX

DIN 48 × 48-mm Multifunction Digital Timer/2-stage Digital Timer

Other Timers FAQ