Page top

Primary Contents

Question

When the Safety Door Switches are installed, is the direction of installation fixed?

Answer



Since the direction of installation for the Safety Door Switches is not fixed, you can install them in any direction.

Therefore, if they are installed upside down or to a position horizontal with the floor surface, no malfunction occurs.

Recommended Products

D4N

Upgraded Safety Limit Switches Based on the Popular D4D, Providing a Full Lineup Conforming to International Standards

F3SJ Ver.2

The updated F3SJ is even easier to use.

OS3101

Operator Presence Detection in Work Areas with Complex Shapes.

Other Safety Door Switches FAQ