Page top

Primary Contents

Question

What are the adjustable head directions and possible points to insert the operation key for D4DS Safety-door Switches?

Answer



As shown in the following figure, the Head can be adjusted into four directions (directions 1 to 4 in the figure) and the key can be inserted at eight points (points 1 to 8 in the figure).

Recommended Products

D4N

Upgraded Safety Limit Switches Based on the Popular D4D, Providing a Full Lineup Conforming to International Standards

F3SJ Ver.2

The updated F3SJ is even easier to use.

OS3101

Operator Presence Detection in Work Areas with Complex Shapes.

Other Safety Door Switches FAQ