![]()
Global
These are navigation links to move inside this page.
![]()
Quick links to OMRON IA in your country / territory.
Please contact our European headquarters.
Question
What is life expectancy (Power Supplies)?
Answer
Typically, the Power Supplies’ service life depend on the service life of the aluminum electrolytic capacitors used in the Power Supplies. When the Power Supplies are operated under proper conditions, the expected service life can be calculated from the measured electrolytic capacitor temperature. This expected service life is known as the life expectancy.
The calculated life expectancy is not equivalent to the warranty period. The life expectancy is simply the projected service life.
The expected service life calculation assumes the following conditions:
1)Rated input voltage
2)Load rate: 50%
3)Ambient operating temperature: 40°C
4)Standard mounting position
5)Continuous 24 hr/day operation
6)Fan life not included for models equipped with a fan