![]()
Global
These are navigation links to move inside this page.
![]()
Quick links to OMRON IA in your country / territory.
Please contact our European headquarters.
Question
I measured the output voltage with a tester and it is lower than the rated voltage. Can the output voltage be adjusted?
Answer
Although there are +/- output models that cannot be adjusted, the output from most Power Supplies can be adjusted by turning the voltage output adjuster (V.ADJ).
The voltage will increase when the adjuster is turned clockwise.
The voltage will decrease when the adjuster is turned counterclockwise.
The ranges in which the voltage can be adjusted are as follows:
Voltage Adjustment Ranges (Typical Examples)
| Power Supplies | Voltage adjustment range |
| S82J Series | ±10% |
| S82K Series (except S82K-03012/-03024/-05024) | ±10% |
| S82K-03012/-03024/-05024 | -10% to +15% |