![]()
Global
These are navigation links to move inside this page.
![]()
Quick links to OMRON IA in your country / territory.
Please contact our European headquarters.
Question
What is the life expectancy of Power Supplies?
Answer
Power Supplies' lifetime depends on its usage.
The life expectancy also depends on the model of Power Supplies being used, as shown in the following table. Use this information as reference for maintenance and replacement.
Conditions:
1.Input voltage: Rated input voltage
2.Load rate: 50%
3.Ambient temperature: 40°C
4.Mounting: Standard mounting direction
| Life expectancy | Main Models |
| Eight years or longer | S82K |
| Ten years or longer | S82J, S8TS, S8VS, S8VM |
Note:The life expectancy was calculated by high-temperature testing of the aluminum electrolytic capacitor, so these values are guidelines only.
With S8VS Series Switch Mode Power Supply, the Maintenance Forecast Monitor Function will indicate the approximate time remaining until recommended replacement of Power Supplies.
Digital Time Interval Meter for Measuring Passing Speed, Time, or Cycle between Two Points.