![]()
Global
These are navigation links to move inside this page.
![]()
Quick links to OMRON IA in your country / territory.
Please contact our European headquarters.
Question
The output indicator turns ON, but then turns OFF immediately. What is the cause of the problem and solution (in models equipped with the overvoltage protection function)?
Answer
| Likely cause | Solution |
| The remote sensing terminals are open. (Indicates that the remote sensing function is being used.) | When not using remote sensing, short-circuit terminals +V and +S, and also terminals -V and -S. The overvoltage protection function will operate, so turn OFF the input power and then turn it back ON again. ![]() |
| The internal control circuit has malfunctioned, thereby activating the overvoltage protection function. | Turn OFF the input power and then turn it back ON again. If the problem reoccurs, the internal circuits are possibly damaged. Consult your OMRON representative. |