Page top

Lead Contents

FAQ02219 of Thumbwheel Switches FAQ

FAQ No. FAQ02219

Primary Contents


Can we set the digit of the Thumbwheel Switches to be dialed only in the range from 0 to 3?


(1) Any number can be set with the models equipped with external stoppers.

Applicable Model Number: A7BS-20[]-S

(2) The models equipped with internal stoppers are also available.

Applicable Model Number: A7D[],A7B[],A7P[]

Stoppers are attached when the units are assembled in the factory.

The position where stoppers are attached cannot be changed. They are only available by order.

Add the suffix -S[][]to the model number, specifying the range in the blanks.

Example: in the case of the range from 0 to 3: A7PS-203-S03

Recommended Products


Improved Design for a More Lightweight Construction and Reduced Standby Power Consumption.


Best-selling Basic Switch Boasting High Precision and Wide Variety


Wide Range of Two-circuit Switches; Select One for the Operating Environment/Application

Other Thumbwheel Switches FAQ