Page top

Lead Contents

FAQ02279 of Safety Relays FAQ

FAQ No. FAQ02279

Primary Contents


What is an inverse input?


An inverse input is an input that creates a potential difference between two input circuit channels (one input positive and one input negative potential) to ensure that the power is cut and the safety function operates if the wiring is damaged and a short-circuit occurs between the channels.

Recommended Products


For Safety Light Curtain Robust & Basic New Lineup. Understanding the Indicators at a Glance.


Compact (104.5 mm), lightweight (1.3 kg) and easy-to-install Safety Laser Scanner


Supports ISO 13849-1 (PLe/Safety Category 4). Can be used on higher risk level applications by connecting to Safety Controllers.

Other Safety Relays FAQ