Page top

Lead Contents

FAQ02367 of Safety Relays FAQ

FAQ No. FAQ02367

Primary Contents


What is redundancy?


Redundancy is duplication. The probability of hazards arising from one malfunction in an electrical circuit can be minimized by creating partial or complete Redundancy (duplication).

The following diagram shows an example circuit where the use of two or more relays or switches in parallel enables performing the total function if one of them is malfunctioning.

Redundant Circuit Configuration Example Using Two Relays

Redundant Circuit Configuration Example Using Two Switches

Recommended Products


For Safety Light Curtain Robust & Basic New Lineup. Understanding the Indicators at a Glance.


Compact (104.5 mm), lightweight (1.3 kg) and easy-to-install Safety Laser Scanner


Supports ISO 13849-1 (PLe/Safety Category 4). Can be used on higher risk level applications by connecting to Safety Controllers.

Other Safety Relays FAQ