![]()
Global
These are navigation links to move inside this page.
![]()
Quick links to OMRON IA in your country / territory.
Please contact our European headquarters.
Question
Can 61F Floatless Level Controllers be used only for liquid level detection in order to output a signal, without turning a pump ON or OFF?
Answer
Yes, this is possible by disconnecting E2 self-holding circuit.
However, when there are waves on the liquid surface, 61F will also repeatedly turn ON and OFF, so the lifetime of the contacts will be shorter than usual.
61F-G Example
Applicable Models
61F-G/61F-GH/61F-GD/61F-GR/61F-GL 2km/61F-GL 4km/61F-G-TDL/61F-GT
61F-GN/61F-GNH/61F-GND/61F-GNR
61F-GP-N/61F-GP-NL 2km/61F-GP-NL 4km/61F-GP-NH/61F-GP-ND/61F-GP-NR/61F-GP-N8/61F-GP-N8L 2km/61F-GP-N8L 4km/61F-GP-N8H/61F-GP-N8D/61F-GP-N8R
61F-UHS/61F-GP-N15/61F-GPN-BT/61F-GP-N8HY