![]()
Global
These are navigation links to move inside this page.
![]()
Quick links to OMRON IA in your country / territory.
Please contact our European headquarters.
Question
What does the “D2” in MY[]N-D2 General-purpose Relays indicate?
Answer
When transistors are used to operate relays, any effects on the transistor caused by the surge, such as deterioration and breakdown, will be eliminated.
Note:
1.Make sure that the polarity is correct.
2.The reset time will be longer, but it will still be within 20 ms.
3.Diode characteristics:
Reverse breakdown voltage: 1,000 V
Forward current: 1 A