![]()
Global
These are navigation links to move inside this page.
![]()
Quick links to OMRON IA in your country / territory.
Please contact our European headquarters.
Question
What other models can use the same Sockets as the G2R General-purpose Relays?
Answer
Refer to the following table.
Relays (plug-in terminals)
| No. of poles | 1 pole | 2 poles | ||
| Type | Degree of protection | Contact form | Model | Model |
| Standard model | Encased | DT contacts | G2R-1-S | G2R-2-S |
| Built-in operation indicator | G2R-1-SN | G2R-2-SN | ||
| Built-in diode | G2R-1-SD | G2R-2-SD | ||
| In-built operation indicator and diode | G2R-1-SND | G2R-2-SND | ||
Connection Sockets
| Type | Surface-mounting socket | Back-mounting socket | ||
| No. of poles | Applicable Relays | Model | Terminal type | Model |
| 1 | G2R-1-S(N) (D) (ND) | P2RF-05 | PCB terminals | P2R-05P |
| P2R-057P | ||||
| P2RF-05-E | Soldered terminals | P2R-05A | ||
| 2 | G2R-2-S(N) (D) (ND) | P2RF-08 | PCB terminals | P2R-08P |
| P2R-087P | ||||
| P2RF-08-E | Soldered terminals | P2R-08A | ||
Note:
1.These Sockets have lock mechanisms to hold the Relays in place.
2.Sockets with "-E" at the end of the model number have finger protection. Round crimp terminals cannot be used. Use forked crimp terminals.