![]()
Global
These are navigation links to move inside this page.
![]()
Quick links to OMRON IA in your country / territory.
Please contact our European headquarters.
Question
How do the indicators on Photoelectric Sensors operate?
Answer
There is a stability indicator (green) and an incident light indicator (red). There are four operation patterns depending on the amount of incident light.
Explanation:
The stability indicator shows the excess gain for temperature, voltage, dust, or other changes in the environment after installation.
Incident Light Indicator
The incident light indicator shows the amount of light entering the receiver.
Indicator operation
| Incident light (See note.) | Indicator | Status | ||
| Green | Red | |||
| 1 | 1.2 min. | ![]() | ![]() | Stable, light |
| 2 | 1.0 to 1.2 | ![]() | ![]() | Unstable, light |
| 3 | 0.8 to 0.99 | ![]() | ![]() | Unstable, dark |
| 4 | 0.8 max. | ![]() | ![]() | Stable, dark |
Note:The operating level is 1.
The following figure shows indicator operation on a graph.
Standard Sensors for Detecting Ferrous Metals under Standard Conditions
OMRON's Fiber Sensors continue to support an increasing range of applications.
Real color sensors equipped with 2-million-pixel CCDs, the fastest in the industry. Nine different types of cameras are available.