![]()
Global
These are navigation links to move inside this page.
![]()
Quick links to OMRON IA in your country / territory.
Please contact our European headquarters.
Question
What is a Photoelectric Sensor?
Answer
A photoelectric sensor is the one to detect presence and the state of the object by the change in light.
1. What is a photoelectric sensor?
Amount of light (luminance) is converted to an electrical signal, certain standard is set to a level of the electrical signal, the output is ON or OFF whether a level of an electrical signal (amount of light entered) is high or not than the standard.
2. Classification of photoelectric sensor
Standard Sensors for Detecting Ferrous Metals under Standard Conditions
OMRON's Fiber Sensors continue to support an increasing range of applications.
Real color sensors equipped with 2-million-pixel CCDs, the fastest in the industry. Nine different types of cameras are available.