![]()
Global
These are navigation links to move inside this page.
![]()
Quick links to OMRON IA in your country / territory.
Please contact our European headquarters.
Question
What does the reversing polarity of power supply cause?
Answer
Although it differs depending on the model, it doesn't operate at all (it is not destruction) or the operation mode is switched.
1. The sensor is not destroyed because the protection diode against reverse connection is certainly in it.
2. The diode bridge is in the power supply input, and the operation mode is switched. (*1)
(*1.)E3S-GS, E3S-VS, E3L, E3S-R[]E[]series
(Refer to the applicable date sheets for details.)
Standard Sensors for Detecting Ferrous Metals under Standard Conditions
OMRON's Fiber Sensors continue to support an increasing range of applications.
Real color sensors equipped with 2-million-pixel CCDs, the fastest in the industry. Nine different types of cameras are available.