![]()
Global
These are navigation links to move inside this page.
![]()
Quick links to OMRON IA in your country / territory.
Please contact our European headquarters.
Question
What are the methods of mutual interference prevention in through-beam photoelectric sensors?
Answer
Point of mutual interference prevention
The light of other sensor do not enter own receiver.
Prevention methods are as follows.
1. Setting of out of parallel operating range
Please confirm parallel operating range on the catalog, install setting distance of adjacent sensor by 1.5 times min.
2. Alternate arrangement setting of photoelectric sensor
Up to two sets of emitters and receivers can be attached closely as following alternative arrangement.
Condition:
The light of the next emitter might be received when the sensing object is close to the photoelectric sensor.
3. Use of mutual interference prevention filter
By use of mutual interference prevention filter, up to 2 sets can be attached closely.
Mutual interference prevention filters are as follows.
E39-E6 for E3S-A
E39-E8 for E3S-B
E39-E11 for E3Z-T[][]A
4. Mutual interference prevention by adjusting sensitivity
When sensing distance is shorter than rating setting distance, the influence of mutual interference is nothing by lowering sensitivity volume though it depends on the customer applications and the selection models.
Standard Sensors for Detecting Ferrous Metals under Standard Conditions
OMRON's Fiber Sensors continue to support an increasing range of applications.
Real color sensors equipped with 2-million-pixel CCDs, the fastest in the industry. Nine different types of cameras are available.