![]()
Global
These are navigation links to move inside this page.
![]()
Quick links to OMRON IA in your country / territory.
Please contact our European headquarters.
Question
By what principle is the limited reflective Photoelectric Sensor detected?
Answer
In the optical system of the limited reflective sensor, only the regular reflection of a certain limited distance is received because the emitter axis intersects with a receiver axis in the same inclination θ.
In the optical system of the limited reflective sensor, the emitter axis intersects with a receiver axis in the same inclination θ as shown in figure.
Only the regular reflection of a certain limited distance is received with such an optical system.
Therefore, only the object within the range where the emitter axis intersects with a receiver axis will be detected.
Moreover, the distance that reaches the peak of the excess gain never changes by the difference of the color because it uses the regular reflection.
(However, the width of detection shortens by the amount of light reflection decrease.)
Standard Sensors for Detecting Ferrous Metals under Standard Conditions
OMRON's Fiber Sensors continue to support an increasing range of applications.
Real color sensors equipped with 2-million-pixel CCDs, the fastest in the industry. Nine different types of cameras are available.