Page top

Lead Contents

FAQ02058 of Solid-state Relays FAQ

FAQ No. FAQ02058

Primary Contents

Question

We think a Solid-state Relay (SSR) is faulty. Can a voltage tester be used to check an SSR to see if current is flowing?

Answer



No, that is not possible.

The voltage and current in the tester's internal circuits are too low to check the operation of the semiconductor element in the SSR (a triac or thyristor). The SSR can be tested as described below if a load is connected.

Testing Method

Connect a load and power supply, and check the voltage of the load terminals with the input ON and OFF. The output voltage will be close to the load power supply voltage with the SSR turned OFF. The voltage will drop to approximately 1 V with the SSR turned ON. This is more clearly checked if the dummy load is a lamp with an output of about 100 W.

(However, the capacity of the lamp must be within the rated range of the SSR.)

Recommended Products

MY

New Latching Levers for Circuit Checking Added to Our Best-selling MY General-purpose Relays

LY

Power-switching Compact General-purpose Relays

G3PE (Three-phase)

Compact, Slim-profile SSRs with Heat Sinks. Solid State Contactors for Three-phase Heaters Reduced Installation Work with DIN Track Mounting.

Other Solid-state Relays FAQ