Page top

Lead Contents

FAQ02101 of Solid-state Relays FAQ

FAQ No. FAQ02101

Primary Contents


Can a DC load be used with Solid-state Relays for AC loads?


No, it cannot be used. The element characteristics of Solid-state Relays will not allow it to reset if a DC load is used.


Solid-state Relays for AC load switching use thyristors and triacs as output elements. By turning Solid-state Relays input ON, the output can be turned ON, but simply turning the input OFF doesn't mean that the output will be turned OFF. This is because Solid-state Relays have a characteristic that it stays turned ON until the load current becomes zero regardless of the absence of input signals into Solid-state Relays.
The DC current will never become zero, therefore it will not be reset.

Recommended Products


New Latching Levers for Circuit Checking Added to Our Best-selling MY General-purpose Relays


Power-switching Compact General-purpose Relays

G3PE (Three-phase)

Compact, Slim-profile SSRs with Heat Sinks. Solid State Contactors for Three-phase Heaters Reduced Installation Work with DIN Track Mounting.

Other Solid-state Relays FAQ