Page top

Lead Contents

FAQ02106 of Solid-state Relays FAQ

FAQ No. FAQ02106

Primary Contents

Question

The Solid-state Relay (SSR) is too hot to touch. Does it have any trouble?

Answer



Although when the maximum current flows in the rated range, the temperature of the SSR reaches around 80 to 100 degrees, it is not abnormal.

However, pay careful attention to the heat loss. In general, when the ambient temperature is high, the value of switchable load currents decreases.

Switching elements in the SSR such as TRIAC, Thyristor and power transistor produce heat by having residual voltage (voltage lost inside a semiconductor when it turns ON).

Recommended Products

MY

New Latching Levers for Circuit Checking Added to Our Best-selling MY General-purpose Relays

LY

Power-switching Compact General-purpose Relays

G3PE (Three-phase)

Compact, Slim-profile SSRs with Heat Sinks. Solid State Contactors for Three-phase Heaters Reduced Installation Work with DIN Track Mounting.

Other Solid-state Relays FAQ