Page top

Lead Contents

FAQ02129 of Solid-state Relays FAQ

FAQ No. FAQ02129

Primary Contents

Question

What should be done for a surge-absorbing circuit for DC-load Solid-state Relays?

Answer



Countermeasures against DC Switching Output Noise Surges

When an L load, such as a solenoid or electromagnetic valve is connected, connect a diode that prevents counter-electromotive force. If the counter-electromotive force exceeds the withstand voltage of the Solid-state Relay output element, it could result in damage to the Solid-state Relay output element.

As a countermeasure, insert the elements in Figure 1 in parallel with the load. (Refer to the following figure.)

As an absorption element, the diode is the most effective at suppressing the counter-electromotive force. The release time for the solenoid or electromagnetic valve will, however, increase. Be sure to check the circuit before use. To shorten the time, connect a Zener diode and a regular diode in series. The release time will be shortened at the same rate that the Zener voltage (Vz) of the Zener diode is increased.

Figure 1: Absorption Element Example

Absorption element
DiodeDiode + Zener diodeVaristorCR
Effectiveness×

(Reference)

1.Selecting a Diode

Withstand voltage = VRM ≥ Power supply voltage × 2

Forward current = IF ≥ Load current

2.Selecting a Zener Diode

Zener voltage = VZ < (Solid-state Relay's connector − emitter voltage)* − (Power supply voltage + 2 V)

Zener surge reverse power = PRSM > VZ × Load current × Safety factor (2 to 3)

Note:When the Zener voltage is increased (VZ), the Zener diode capacity (PRSM) is also increased.

Recommended Products

MY

Best-selling, general-purpose relays that can be selected based on operating environment and application

LY

Power-switching Compact General-purpose Relays

G3PE (Three-phase)

Compact, Slim-profile SSRs with Heat Sinks. Solid State Contactors for Three-phase Heaters Reduced Installation Work with DIN Track Mounting.

Other Solid-state Relays FAQ