![]()
Global
These are navigation links to move inside this page.
![]()
Quick links to OMRON IA in your country / territory.
Please contact our European headquarters.
Question
The Reflector is fogged up. Is there any way to improve the situation?
Answer
Use E39-R1K Reflectors with a anti-fog coating. Regular Reflectors become fogged up when the temperature changes from -5°C to room temperature. Reflectors with anti-fog coating can withstand temperature changes from -25°C to room temperature.
Standard Sensors for Detecting Ferrous Metals under Standard Conditions
OMRON's Fiber Sensors continue to support an increasing range of applications.
Real color sensors equipped with 2-million-pixel CCDs, the fastest in the industry. Nine different types of cameras are available.