![]()
Global
These are navigation links to move inside this page.
![]()
Quick links to OMRON IA in your country / territory.
Please contact our European headquarters.
Question
What role does the Slit play for Through-beam Photoelectric Sensors and how is it used?
Answer
Role of Slit
The Slit is mounted on the emitter and receiver of Through-beam Photoelectric Sensors to decrease the lens diameter and narrow the light beam. This is done to increase the sensing performance for the smallest detectable object.
Usage
One set of two Slits for the emitter and receiver is generally used mounted to the emitter and receiver of a Through-beam Photoelectric Sensor. It is also possible, however, to use a Slit on only either the emitter or the receiver, depending on the sensing distance and the size of the sensing object.
Slits, however, cannot be used on Reflective Photoelectric Sensors (e.g., Retroreflective, Diffuse-reflective, Convergent-reflective, or Distance-settable Sensors).
Standard Sensors for Detecting Ferrous Metals under Standard Conditions
OMRON's Fiber Sensors continue to support an increasing range of applications.
Real color sensors equipped with 2-million-pixel CCDs, the fastest in the industry. Nine different types of cameras are available.