![]()
Global
These are navigation links to move inside this page.
![]()
Quick links to OMRON IA in your country / territory.
Please contact our European headquarters.
Question
What are the differences between E39-R1 General-purpose Reflectors and E39-R1K Reflectors with anti-fog coating?
Answer
E39-R1K Reflectors are the same as E39-RQ, except they have an anti-fog coating added to the reflective surface. The anti-fog effect of the coating is similar to that used by ski goggles.
The sensing distance with E39-R1K is the same as with E39-R1. For example, with E3Z-R Photoelectric Sensors with built-in amplifier, the sensing distance is 3 m whether E39-R1 or E39-R1K is used.
Standard Sensors for Detecting Ferrous Metals under Standard Conditions
OMRON's Fiber Sensors continue to support an increasing range of applications.
Real color sensors equipped with 2-million-pixel CCDs, the fastest in the industry. Nine different types of cameras are available.