![]()
Global
These are navigation links to move inside this page.
![]()
Quick links to OMRON IA in your country / territory.
Please contact our European headquarters.
Question
Which hole of the Amplifier Unit can the Through-beam Fiber Unit be inserted into?
Answer
It makes no difference which hole it is inserted into, because there is no distinction between the two fibers for a Through-beam Fiber Unit.
With a Coaxial Diffuse-reflective Fiber Sensors (such as the E32-C31), the holes that the fibers are inserted into are set for the receiver and emitter.
Standard Sensors for Detecting Ferrous Metals under Standard Conditions
OMRON's Fiber Sensors continue to support an increasing range of applications.
Real color sensors equipped with 2-million-pixel CCDs, the fastest in the industry. Nine different types of cameras are available.