![]()
Global
These are navigation links to move inside this page.
![]()
Quick links to OMRON IA in your country / territory.
Please contact our European headquarters.
Question
What is the cable length of the D9M Safety Mat? Can it be extended?
Answer
The cable length of the D9M is 3 m. (No other lengths are available.) It can be extended, but the maximum length is 100 m. (There are two lead wires per cable so the total maximum length of the lead wires is 200 m.)
There are no specific requirements for the extension cable, but it is recommended that you use the same type of cable as the one that is attached to the D9M (0.75 mm2) or thicker.
Upgraded Safety Limit Switches Based on the Popular D4D, Providing a Full Lineup Conforming to International Standards
The updated F3SJ is even easier to use.
Operator Presence Detection in Work Areas with Complex Shapes.