Page top

Lead Contents

FAQ00861 of Timers FAQ

FAQ No. FAQ00861

Primary Contents

Question

What will happen to the H5S, H5F, or H5L Time Switches if power is interrupted?

Answer



If power is interrupted to the H5S, H5F, or H5L Time Switch, the output will turn OFF and the display will go black.

The present clock time and program contents, however, will be saved.

Example: Power interruption compensation for the H5S Electrical Time Switch.

Lithium battery:

Continuous operation: 5 years min. (at 25°C)

10 years min. (at 25°C, power interruption ratio of 50% max.: Total time that power is stopped.)

Description

The H5S uses a lithium battery for memory backup for power interruptions.

At an ambient temperature of 25°C, the present clock data and setting contents will be saved for a total power interruption time of 5 years max.

"10 years min. (power interruption ratio of 50%)" means a total of 10 years comprised of 5 years total power ON time and 5 years total power interruption time. (Battery power is not consumed while power is being applied.)

Note: When the H5S is used, the output will not operate and the display will not be shown during power interruptions.

The power interruption compensation function saves the internal clock data and settings only, so the output circuit remains OFF.

Recommended Products

K3HB-X

A Process Indicator Ideal for Discriminating and Displaying Measurements for Voltage/Current Signals

E5CN-H

A New High-performance Controller: High Resolution, High Speed, and High Input Accuracy. Logic Operations and Preventive Maintenance Function.

H5CZ

Easy to Use and Easy to Read.

Other Timers FAQ