![]()
Global
These are navigation links to move inside this page.
![]()
Quick links to OMRON IA in your country / territory.
Please contact our European headquarters.
Question
Are there any specific application methods that will extend the life of an Axial-flow Fan?
Answer
Yes, the following methods will help extend the lifetime.
1.Keep the ambient temperature (i.e., temperature of the Fan itself) as low as possible.
→ Use the Fan at the inlet.
2.Do not subject the Fan to shock. (The bearing is especially susceptible to damage from shock and has a major effect on the Fan life.)
3.As much as possible, do not expose the Fan directly to dust and other airborne particles.
→ Install a filter.