This is the difference in pressure between the inside of a flowrate meter and the outside air pressure when the flowrate is set to 0 m3/min. In other words, it is the pressure at the front of the Fan when the Fan front is made completely airtight and the Fan is operated.