Page top

Lead Contents

FAQ03000 of Timers FAQ

FAQ No. FAQ03000

Primary Contents


What is the difference between the Timer and the Time Switch?


The Timer controls the time from when the power is turned on or the input signal is supplied to when the operation starts. On the other hand, the Time Switch controls the time of day at which the operation starts with the power on.

Recommended Products


A Process Indicator Ideal for Discriminating and Displaying Measurements for Voltage/Current Signals


A New High-performance Controller: High Resolution, High Speed, and High Input Accuracy. Logic Operations and Preventive Maintenance Function.


Easy to Use and Easy to Read.

Other Timers FAQ