Page top

Lead Contents

FAQ03045 of Timers FAQ

FAQ No. FAQ03045

Primary Contents


Which timer can be used as a substitute product for ATSS Pneumatic OFF-delay Timers?


H3CR Solid-state Timers.
ATSS Timers have either power ON-delay or power OFF-delay operation. The substitute products depends on which type of ATSS were used.

Example: Replacing ATSS 24VDC 10S OFF

ATSS Timers operate with a supply voltage of 24 VDC and a power OFF-delay of 10 seconds. A substitute product for this timer is H3CR-H8L 24 VAC/VDC S.
H3CR-H8L does not have instantaneous contacts. If instantaneous contacts are required, a relay must be connected externally. The "S" after the voltage indicates a time range of 0.05 s to 12 s.


*These dimensions vary with the kind of DIN track (reference value).

Note:The terminal arrangement is the same, but the outputs are both subject to limit resetting.

Recommended Products


A Process Indicator Ideal for Discriminating and Displaying Measurements for Voltage/Current Signals


A New High-performance Controller: High Resolution, High Speed, and High Input Accuracy. Logic Operations and Preventive Maintenance Function.


Easy to Use and Easy to Read.

Other Timers FAQ